Dehumidification Control Configuration
Notes
- Dehumidification control is a mode of Cooling when hot gas reheat is configured.
- Relative Humidity uses a humidity sensor connected to UC-J23.https://support.trane.com/hc/en-us/articles/4544884023693-How-do-I-wire-a-BAYSENS036-037-Humidity-Temp-Sensor-for-Symbio-700-and-Reliatel-Controls
Humidistat connects to the Customer Connection Module (CCM) on CCM-J3 terminals 1 and 2.
Configure as follows
- Go to Settings > View Configuration
- Top right-corner Edit
- Change Dehumidification Control from Relative Humidity to Humidistat
- Change or verify the Humidistat is to Install
- Change Humidity Sensor to Not Install
- Press Save on the top right-corner to save the configurations
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.