Sequence of Operation
Initiation
When Humidistat input is used, dehumidification initiates when the Symbio 700 Humidistat input becomes active (24vac present on Customer Connection Module J3-2). A Y1 call is not required to initiate dehumidification.
If there is no thermostat call for cooling, heating, or supply fan, the unit will be off. When the Humidistat input is active, the Symbio 700 controller will start the unit and provide dehumidification.
When dehumidification activates, compressors stage to full capacity, economizer cooling is disabled. The reheat valve will open targeting the max allowed position, then modulate to an adjustable Discharge Air Reheat Setpoint (70°F default). This setpoint is adjustable in the Symbio Service & Installation Mobile App in SETTINGS → REFRIGERATION → DISCHARGE AIR REHEAT SETPOINT BAS and has an adjustable range between 65°F & 80°F.
Termination
Any condition listed below will terminate dehumidification:
- Humidistat input opens
- Thermostat Y1 + Y2 call (dehumidification is allowed with a Y1 OR Y2 only call)
- Thermostat Heat Call
- Occupancy Input Closes and Unoccupied Dehumidification is disabled
- Entering Evaporator Temperature below 30°F or failed Entering Evaporator Temperature Sensor
- Outdoor Air Temperature below 40°F or above 100°F
- Stepper Motor Module (SMM) communication failure
- Any emergency stop condition that stops the compressors or supply fan
Wiring
Troubleshooting
Unit will not enter dehumidification
- Is the OAT between 40°F and 100°F ?
- Once the OAT exceeds these values, there is a 5°F dead band to allow dehumidification to work again, OAT would have to be >45°F or <95°F to re-enable dehumidification
- Does the unit have Y1 + Y2 calls ?If the Y2 call drops, the dehumidification will begin per the normal sequence of operations
- Is the thermostat calling for Heat ?A call for heat will disable dehumidification instantly
- Is 24vac present on Customer Connection Module J3-2 Humidistat Input
Unit overheating the space
- Typically a thermostat will stop this from happening when the Y2 calls is added, but the Discharge Air Reheat Setpoint BAS (default 70°F) may be set too high for the space and is add too much heat during dehumidification.
- If you have a single stage cooling unit (Standard Efficiency 3-5T) and only have a Y1 call wired to the unit, the same scenario above could be in play and there is not a Y2 call to terminate dehumidification. Adding a Y2 call to a single stage unit is a good idea for space temperature protection during dehumidification, but also the Y2 call is needed during economizer operation to allow the compressor to operate to supplement the outdoor air damper.
Unit overcooling the space
- If the Discharge Air Reheat Setpoint BAS is set to the minimum of 65°F, it may be providing enough cooling to allow the space temperature to drop.
Symbio 700 Dehumidification Points
Values in ORANGE are adjustable
| BACnet Instance | Point Name | Default | Range | Use | App/User Interface Location |
|---|---|---|---|---|---|
| AI-10124 | Discharge Air Temperature Local | -- | Local Discharge Air Temperature | STATUS>INDOOR | |
| AI-11166 | Evaporator Entering Refrigerant Temperature | -- | Local Evaporator Entering Refrigerant Temperature (located on leaving side of TXV) | STATUS>REFRIGERATION | |
| AI-11164 | Reheat Valve 1 Step Status | -- | Reheat Valve Steps (0 = Closed) | STATUS>REFRIGERATOIN | |
| AV-10134 | Discharge Air Reheat Setpoint BAS | 70°F | 65°F-80°F | DAT Target Setpoint while in reheat (controls HGRH valve Modulation) | SETTINGS>REFRIGERATION |
| AV-11281 | Dehumidification Control Status | 0% | HGRH Valve Position in % | STATUS>REFRIGERATION | |
| AV-11315 | Reheat Purge Interval (minutes) | 120 | 60-180 | Amount of continuous reheat operation before 3 min purge/compressor cool down sequence | SETTINGS>REFRIGERATION |
| BI-11143 | Reheat Humidistat Input | -- | Status of Customer Connection Module J3-2 Humidistat Input | STATUS>SYSTEM | |
| BI-11187 | Reheat Pumpout Solenoid Status | -- | Status or Reheat Pumpout Solenoid Command, Solenoid is off during dehum, on during normal cooling | STATUS>SYSTEM | |
| BV-10106 | Dehumidification Enable Command | Auto | Auto, Disabled | Setting to Disabled will disable all dehumidification efforts. | SETTINGS>REFRIGERATION |
| BV-11255 | Dehumidification Status | Inactive | Status of unit dehumidification control | STATUS>REFRIGERATION | |
| BV-11259 | Occupied Dehumidification Enable BAS | Enabled | Enabled, Disabled | Allows unit to dehumidify when the unit is occupied (J20-2 = Open). | SETTINGS>REFRIGERATION |
| BV-11261 | Unoccupied Dehumidification Enable BAS | Enabled | Enabled, Disabled | Allows unit to dehumidify when the unit is unoccupied (J20-2 = Closed/24vac present) | SETTINGS>REFRIGERATION |
- Other dehumidification/reheat points are available in the mobile app, these points either do not affect thermostat with humidistat control, are feedback/active values or are not recommend to be changed without Tech Support direction.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.