Unit Auto
Connect to your Symbio Service and Installation App.
- Navigate to the TOOLS section of the phone app
- Below Tools, there it will be the first selection as Unit Auto/Stop with a toggle feature to the right indicating its current position
Refer to the image below for the unit being in Auto mode:
Unit Stop
The Unit Stop feature allows for immediate shutdown of all devices in the equipment when initiated.
When a Unit Stop request is received, the following actions are taken:
- All equipment control binary outputs are de-energized
- Indoor fan
- Compressors
- Condenser fans
- Unloader solenoids
- Heat stages
- All equipment control analog outputs are set to their minimum/off command values.
- All communicating devices, such as supply fans, are commanded to their off state.
- All control algorithms are initialized to their normal startup values and held until the stop request is released.
To change the unit to stop mode
- Click on the Toggle that says Auto in grey, and the image below will appear:
Click Proceed to stop the equipment.
Refer to the image below to determine if your unit is in Stop mode:
- When the toggle is to the right and in blue, the unit is in Stop mode.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.