0 to 50% Motorized Outside Air Damper
Used With
| Model Numbers: | Used With: |
|---|---|
FIADMPR101* |
Precedent A cabinet (Digit 39 = A) |
FIADMPR102* |
Precedent B and C cabinet (Digit 39 = B, C) |
FIADMPR103* |
Precedent D cabinet (Digit 39 = D) |
Installation Instructions Manual
Click the e-library symbol for the latest version of the 0 to 50% Motorized Outside Air Damper.
Wiring
- Using the supplied harness, connect PPF87 to the actuator connector.
- Route the harness to the fresh air options module located in the return section and connect to the blue connector to P11 and the black connector to P8.
Configuration
- Click the link below to configure or edit the configurations.
Phone App
- Click Settings > View Configuration > Edit > Proceed, then edit the required configurations.
Using the Symbio 700 Onboard menu and keypad
- Press Home.
- Press the Down Arrow and select Utilities.
- Press the Check.
- Press the Down Arrow and select Unit Config.
- Press the Check.
- Press the Down Arrow and select Edit Unit Config.
- Press the Check.
- Press the Down Arrow, then select Outside Air.
- Press the Check.
- Press the Down Arrow, and select 0 to 50% Motorized Damper.
- Press the Down Arrow, then verify that the Remote Minimum Position is Not Installed.
- Or Press the Check.
- And select Not Installed.
- Press the Check.
- Press the Down or Up Arrow until you find Save Config.
- Press the Check.
- Press the Down Arrow to change No to Yes.
- Press the Check.
- It will say Edit Unit Config Updating.
Minimum Position Setting
- When a 0 to 50 percent motorized damper is installed, with any supply fan type, the outdoor air damper is controlled to a setpoint from a Remote Minimum Position (wired input), Motorized Damper Position Setpoint, or Economizer Minimum Position Setpoint BAS. The following table summarizes which setpoint controls the damper position based on the installed and enabled options.
| Supply Fan Compensation | Remote Minimum Position | Occupancy Status | Outdoor Air Damper Controlling Setpoints |
| Enabled | Installed | Any | Remote Minimum Position |
| Enabled | Not Installed | Any | Motorized Damper Position Setpoint |
| Disabled | Installed or Not Installed | Any | Economizer Minimum Position Setpoint BAS |
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.