There are times when a technician would like to test VFD operation or fan performance by placing the VFD in the Hand Mode. From the factory this feature is DISABLED because it takes away the ability for the unit to control the VFD during normal operation, VOM override, Emergency Stop and/or Equipment Stop command. Symbio 700 and 800 units communicate through Modbus communication therefore the Modbus Control Source parameter must be changed as well.
How to change TR150 VFD parameters on IntelliPak and Voyager 3
- Enable Hand Mode
- Change parameter 0-40 from Disabled [0] to Enabled [1].
- Change parameter 8-02 from FC Port [1] to None [0].
-
Press Hand Key - should be able to ramp the fan Hz up and down with arrow keys.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.