Purpose
This article uses generic diagram and electric panel layouts to illustrate how the multi-speed fan functions. This may be used to help verify wiring and component issues in the field in the event the supply fan isn't functioning properly.
Resolution
The screen shots contained in this article are generic. See your unit electric diagram for specific wiring.
There are two different overloads for high (HS/OL) and low speed (LS/OL) fan which are manual reset. See the motor starter locations below for location information and verify the overload isn't tripped.
Fan speed control is accomplished using motor starters which jump together different motor leads to stage the fan from Low to High speed.
There are multiple ways to command the fan speed manually.
- Tracer TU: Commissioning Mode for UC400 & Symbio 400/500 in TU
- Web UI (Symbio 400-B and 500 only): How do you manually test outputs using the Symbio Web UI on a WSHP?
- Manual Test Button: How do you use the service pin to test outputs UC400 & Symbio 500 / 400-B?
WARNING
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.