Qualified service technician or installer may activate all functions of the unit, regardless of thermostat, sensor values using the Symbio Web UI.
| 1. | Using the USB A to B cable, connect your PC to the USB port on the Symbio controller. | |
| 2. | Open a web browser and enter 198.80.18.1 into the address field. Select Login and follow the prompts. | |
| 3. | Select Points from the panel to the left. | |
| 4. | Select Multistate Points from the header towards the center of the window. | |
| 5. | Enter the word "Manual" to filter the point names. | |
| 6. | Left click the blue Manual Test Sequence text. | |
| 7. | Left click the grey down arrow. An Override Manual Test Sequence window will pop up, select the "Change the value anyway button" to continue. | |
| 8. |
Select the desired manual operator state from the dropdown list. Select the Apply button in the lower right to send the value to the control. All possible unit configurable overrides will be shown here regardless of what your unit may have installed. |
|
| 9. |
As default, changes will expire after 2 hours. Unit safeties such as high and lower pressure are still in play and may limit unit operations. To exit manual operation, select the check box to the left of the overridden value followed by the release button. |
WARNING
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.