The red service LED on the LCI communicating interface indicates a fault condition. When it is on continuously or fleshing once every second, it suggest a general fault in the system. This could be due to various reasons suck a communication issues, power supply problems or a fault with the board itself
The applicationless status in Rover Software is kind of a misnomer. It doesn't mean that the board has lost its application software (i.e. it needs to be flash downloaded with an image), it means that the communication state of the LonTalk node is applicationless.
For the board to communicate and function, we need the node state to be configured/online. You can try putting Rover in the Active mode to change the node state. If that doesn't work and you have Node Util or NLUtil, you can use those tools to attempt to change the node state.
See steps on the following article LonTalk device in unconfigured state or Red service LED flashing
If you cannot get the board to report configured and online, replace the board.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.