With a recent motor upgrade there have been reported differences in the motor FLA verses what the nameplate indicates.
NOTE: As long as the Motor FLA is equal or less than the UNIT nameplate, then it is satisfactory to UL standards.
Example:
Unit data tag shows the motor FLA=5.5 however the data tag on the motor shows FLA=4.3.