By following these steps, you should be able to successfully replace your TCI-3 UCP Voyager with the TCI-R ReliaTel Voyager. Remember to exercise caution, adhere to safety guidelines and seek professional assistance if necessary.
TCI-R ReliaTel Comm 3/4 Communication Interface
TCI-R DIP Switch Address Settings
- The DIP switch (SW1) is located on the left corner of the Comm 3/4 board. DIP switches SW1-1 through SW1-5 are used to set the Comm 3/4 board addresses.
TCI-3 UCP Comm 3/4 Communication Interface
TCI-3 DIP Switch Address Settings
The DIP switch (SW1) is located on the upper right corner of the TCI-3 board. DIP switch SW1-1 is used to enable (ON) or disable (OFF) the optional High Temperature Limit Switch binary input (Tb2 on the TCI-3 board).
DIP switches SW102 through SW1-6 are used to set the Voyager Micro Rooftop TCI-3 addresses.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.