Make sure to refer to the user manual or documentation for the TD5 or contact Technical Support for more specific instructions.
To export graphical data from the Td5, you can follow these steps:
- Locate the USB Port on the bottom of the TD5.
- Insert the jump drive into the USB port.
- Next, select the Settings button on the display. Once selected you should see the following page. Once on the Settings page, find and select the Backup and Restore tab.
- Now, select Save Graph Data to USB option.
- Once Save Graph to USB has been selected, a dialogue box should be visible. Please select Yes to confirm the operation.
- If the graph was saved successfully to the USB jump drive, you should see the following dialogue box. Save complete, You may now remove the USB device.
- Press OK and remove the jump drive.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.