- The NOx burner assembly is factory set for optimum performance and should only be adjusted or modified by a qualified technician.
- The burner box and premix/blower valve are mated parts - if either part needs replacing the complete assembly will need to be replaced.
- The low-temperature cutoff switch is intended to prevent gas heat operation below 32°F due to low operating temperature limitations with the premix blower component.
- The NOx gas furnace option is not available for high-altitude installations above 2000 ft.
- Manifold pressure is not applicable for units with the Low NOx Gas furnace option. Manifold pressure is not utilized as an adjustment/checking parameter for this system.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.