- TCO1 = CNT04822 or X13100435030
- TCO2 = CNT03511 or X13100414010
- Flame Rollout Switch = SWT04535 or X13104012001
- Low Temp Sensor (VTL) = SEN03030 or 436801490001
- Pressure Switch = CNT03520 or X13240405010
- Power Supply 24VAC to 24VDC (PWR1) = BRD05110 or X13651580010
- Control Relay (NOX1) = RLY03065 or X13300620020
- Transformer 150VA = TRR03076 or X13550968001
- 2 Burner Box 60K B CAB = BOX04282 or 436801270001
- 2 Burner Box 60K C CAB = BOX04283 or 436802140001
- 3 Burner Box 90K C CAB = BOX04284 or 436801280001
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.