Symbio 700Lifting and RiggingSymbio PrecedentTSJTHKTZKWSJYSKYZKDHJDSKDHKTHJTSKWHJWHKYHJYHK3-25 Ton
Below are some of the contents from the IOM: Packaged Rooftop Air Conditioners Precedent™ Cooling and Electric Heat.
Find the full version of the IOM attached below as RT-SVX070C-EN_05302023.pdf.
⚠️ WARNING
Heavy Object!
Failure to follow instructions below could result in unit dropping which could result in death or serious injury, and equipment or property-only damage.
Ensure that all the lifting equipment used is properly rated for the weight of the unit being lifted. Each of the cables (chains or slings), hooks, and shackles used to lift the unit must be capable of supporting the entire weight of the unit. Lifting cables (chains or slings) may not be of the same length. Adjust as necessary for even unit lift.
⚠️ WARNING
Improper Unit Lift!
Failure to properly lift unit in a LEVEL position could result in unit dropping and possibly crushing operator/technician which could result in death or serious injury, and equipment or property-only damage.
Test lift unit approximately 24 inches (61 cm) to verify proper center of gravity lift point. To avoid dropping of unit, reposition lifting point if unit is not level.
Figure 26. Rigging and center of gravity — 6 to 12.5 tonsFigure 27. Rigging and center of gravity — 15 to 25 tons
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.