Used With:
| Model Number: | Used With: |
|---|---|
| FIAHZDC001* | Precedent D cabinet (Digit 39 = D) |
Notes:
There are two sheet metal assemblies that can be used in the unit without any additional preparation work:
- Return duct cover – includes fiberglass insulation
- Supply duct cover – includes insulation, gasket, and bracket attached to the panel. Figure 1 shows both assemblies.
Horizontal Economizer Conversion Kit
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.