- This is the wired controller, with the flip cover.
- If a timer appears on the controller this will require a Factory reset.
- Press and hold either set and delete or Set and Esc. until a 1 appears.
- Up or down make the 1 a 0, arrow to your right, up or down make the 0 a 1, then press set.
- This will restore to Factory settings; you will need to change Celsius to Fahrenheit.
- Temperature to Wired remote controller, if you are reading from the controller.
Wired Remote Controller
Articles in this section
- COMPRESSOR CHANGE OUT PROCEDURE
- REPLACING THE MAIN CONTROL BOARD
- E-206/C001/C002/C003/4
- VRF PRODUCT OPTION CODES
- E-163
- Trane/Samsung Prospace Wireless remote
- VRF Application Guide
- VRF Firmware for 2017 Next Generation Products
- Mode Control Unit (MCU)
- VRF TOUCHSCREEN CONTROLLER