Take a look at the image below for the Temperature and Refrigerant Leak detection sensor location in the condenser and evaporator cabinets.
- There are two refrigerant leak detectors on gas heat units only.
- Cooling / Electric heat only has one located in the return cabinet.
Sensors located in Evaporator section
- T1
- T2A & T2B
- Refrigerant Leak Sensor
(Gas heat units only include another sensor in heat section)
Evaporator Section
View from horizontal opening.
Sensor located in Condenser section
- T3A & T3B
- T4
- T5A & T5B
- Refrigerant Leak Sensor (with gas heat)
Condenser Section
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.