Control Wiring
DPB52 - True RMS 3-Phase, Multifunction monitoring relay True RMS
Connections
- Connect the 3-phase power supply taking care of the sequence.
- Connect the relay output according to the ratings.
- Automatic screwdriver can be used with max. tightening torque:
- L1, L2, L3: 0.4Nm to 0.8Nm
- 15, 16, 18: 0.4Nm to 0.8Nm
Input range and functions settings
- As shown in below turn the Dial “Un” to select the proper monitored mains rated voltage.
- Adjust dial “U<” to set the required Undervoltage percentage related to mains rated value.
- Adjust dial “U>” to set the required Overvoltage percentage related to mains rated value.
Adjust dial “DELAY” to set the delay on alarm activation.
Startup and adjustment
- Check correct setting of input range according to supply.
- Turn power ON.
- If all phases are present, the phase sequence is correct and the phase voltages are all within the set limits, the bi-colour LED Green/Red is GREEN ON steady (No active alarms and no pending ones) Relay #15 to #18 closes and Yellow LED is ON.
The relay releases (200ms delay occurs) when one or more phase voltages fall below 75% of nominal voltage, the phase sequence is not correct or one or more phase voltages exceed the set over / under voltage limits, Relay #15 to #18 opens, Yellow LED turns off and the “AL” LED will show the type of failure occurred.
"AL" LED Status Green ON OK Green flashing DELAY elapsing Red, 1 flash Parameters out of range Red, flashes Wrong phase sequence Red, 3 flashes Phase loss Red, 4 flashes Undervoltage Red, 5 flashes Overvoltage
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.