This purpose of this article is to show how the Medium Foundation unit crankcase heaters are controlled.
The crankcase heaters are controlled off the temperature of the T5 Discharge sensors. If either of the T5A / T5B sensor on Circuit A or Circuit B reads less than 41℉ that circuits compressor crankcase heater will energize.
If either of the T5A / T5B sensor on Circuit A or Circuit B reads more than 45℉ that circuits compressor crankcase heater will de-energize.
On power up of the unit disconnect the crankcase heaters are in standby for up to 3hrs.
Location of T5 Sensors
Temperature sensor OHM / Temperature chart
T5 Temperature Sensor
| °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 0 | -17.8 | 492.753 | 39 | 3.9 | 146.983 | 78 | 25.6 | 52.254 | 117 | 47.2 | 21.366 | 156 | 68.9 | 9.784 | 195 | 90.6 | 4.918 | 234 | 112.2 | 2.670 |
| 1 | -17.2 | 476.483 | 40 | 4.4 | 142.848 | 79 | 26.1 | 50.987 | 118 | 47.8 | 20.915 | 157 | 69.4 | 9.603 | 196 | 91.1 | 4.837 | 235 | 112.8 | 2.631 |
| 2 | -16.7 | 460.817 | 41 | 5.0 | 138.845 | 80 | 26.7 | 49.755 | 119 | 48.3 | 20.475 | 158 | 70.0 | 9.425 | 197 | 91.7 | 4.758 | 236 | 113.3 | 2.593 |
| 3 | -16.1 | 445.730 | 42 | 5.6 | 134.970 | 81 | 27.2 | 48.557 | 120 | 48.9 | 20.045 | 159 | 70.6 | 9.261 | 198 | 92.2 | 4.680 | 237 | 113.9 | 2.556 |
| 4 | -15.6 | 431.200 | 43 | 6.1 | 131.218 | 82 | 27.8 | 47.392 | 121 | 49.4 | 19.626 | 160 | 71.1 | 9.081 | 199 | 92.8 | 4.604 | 238 | 114.4 | 2.518 |
| 5 | -15.0 | 417.202 | 44 | 6.7 | 127.584 | 83 | 28.3 | 46.260 | 122 | 50.0 | 19.217 | 161 | 71.7 | 8.915 | 200 | 93.3 | 4.529 | 239 | 115.0 | 2.482 |
| 6 | -14.4 | 403.717 | 45 | 7.2 | 124.065 | 84 | 28.9 | 45.158 | 123 | 50.6 | 18.818 | 162 | 72.2 | 8.752 | 201 | 93.9 | 4.456 | 240 | 115.6 | 2.446 |
| 7 | -13.9 | 390.722 | 46 | 7.8 | 120.656 | 85 | 29.4 | 44.087 | 124 | 51.1 | 18.429 | 163 | 72.8 | 8.593 | 202 | 94.4 | 4.384 | 241 | 116.1 | 2.410 |
| 8 | -13.3 | 378.198 | 47 | 8.3 | 117.354 | 86 | 30.0 | 43.045 | 125 | 51.7 | 18.049 | 164 | 73.3 | 8.437 | 203 | 95.0 | 4.313 | 242 | 116.7 | 2.376 |
| 9 | -12.8 | 366.127 | 48 | 8.9 | 114.154 | 87 | 30.6 | 42.031 | 126 | 52.2 | 17.678 | 165 | 73.9 | 8.285 | 204 | 95.6 | 4.244 | 243 | 117.2 | 2.342 |
| 10 | -12.2 | 354.489 | 49 | 9.4 | 111.054 | 88 | 31.1 | 41.045 | 127 | 52.8 | 17.316 | 166 | 74.4 | 8.135 | 205 | 96.1 | 4.176 | 244 | 117.8 | 2.308 |
| 11 | -11.7 | 343.269 | 50 | 10.0 | 108.050 | 89 | 31.7 | 40.085 | 128 | 53.3 | 16.963 | 167 | 75.0 | 7.989 | 206 | 96.7 | 4.110 | 245 | 118.3 | 2.276 |
| 12 | -11.1 | 332.450 | 51 | 10.6 | 105.138 | 90 | 32.2 | 39.151 | 129 | 53.9 | 16.618 | 168 | 75.6 | 7.846 | 207 | 97.2 | 4.044 | 246 | 118.9 | 2.243 |
| 13 | -10.6 | 322.015 | 52 | 11.1 | 102.316 | 91 | 32.8 | 38.242 | 130 | 54.4 | 16.281 | 169 | 76.1 | 7.706 | 208 | 97.8 | 3.980 | 247 | 119.4 | 2.211 |
| 14 | -10.0 | 311.949 | 53 | 11.7 | 99.580 | 92 | 33.3 | 37.357 | 131 | 55.0 | 15.952 | 170 | 76.7 | 7.569 | 209 | 98.3 | 3.917 | 248 | 120.0 | 2.180 |
| 15 | -9.4 | 302.239 | 54 | 12.2 | 96.927 | 93 | 33.9 | 36.496 | 132 | 55.6 | 15.630 | 171 | 77.2 | 7.434 | 210 | 98.9 | 3.856 | 249 | 120.6 | 2.150 |
| 16 | -8.9 | 292.870 | 55 | 12.8 | 94.355 | 94 | 34.4 | 35.658 | 133 | 56.1 | 15.317 | 172 | 77.8 | 7.303 | 211 | 99.4 | 3.795 | 250 | 121.1 | 2.119 |
| 17 | -8.3 | 283.828 | 56 | 13.3 | 91.861 | 95 | 35.0 | 34.842 | 134 | 56.7 | 15.010 | 173 | 78.3 | 7.174 | 212 | 100.0 | 3.736 | 251 | 121.7 | 2.090 |
| 18 | -7.8 | 275.102 | 57 | 13.9 | 89.442 | 96 | 35.6 | 34.047 | 135 | 57.2 | 14.711 | 174 | 78.9 | 7.048 | 213 | 100.6 | 3.677 | 252 | 122.2 | 2.061 |
| 19 | -7.2 | 266.679 | 58 | 14.4 | 87.096 | 97 | 36.1 | 33.274 | 136 | 57.8 | 14.419 | 175 | 79.4 | 6.924 | 214 | 101.1 | 3.620 | 253 | 122.8 | 2.032 |
| 20 | -6.7 | 258.546 | 59 | 15.0 | 84.820 | 98 | 36.7 | 32.520 | 137 | 58.3 | 14.133 | 176 | 80.0 | 6.804 | 215 | 101.7 | 3.564 | 254 | 123.3 | 2.004 |
| 21 | -6.1 | 250.696 | 60 | 15.6 | 82.612 | 99 | 37.2 | 31.787 | 138 | 58.9 | 13.854 | 177 | 80.6 | 6.686 | 216 | 102.2 | 3.509 | 255 | 123.9 | 1.976 |
| 22 | -5.6 | 243.115 | 61 | 16.1 | 80.469 | 100 | 37.8 | 31.072 | 139 | 59.4 | 13.582 | 178 | 81.1 | 6.569 | 217 | 102.8 | 3.455 | 256 | 124.4 | 1.949 |
| 23 | -5.0 | 235.792 | 62 | 16.7 | 78.390 | 101 | 38.3 | 30.376 | 140 | 60.0 | 13.315 | 179 | 81.7 | 6.455 | 218 | 103.3 | 3.402 | 257 | 125.0 | 1.922 |
| 24 | -4.4 | 228.719 | 63 | 17.2 | 76.372 | 102 | 38.9 | 29.698 | 141 | 60.6 | 13.055 | 180 | 82.2 | 6.344 | 219 | 103.9 | 3.349 | 258 | 125.6 | 1.895 |
| 25 | -3.9 | 221.886 | 64 | 17.8 | 74.414 | 103 | 39.4 | 29.037 | 142 | 61.1 | 12.801 | 181 | 82.8 | 6.235 | 220 | 104.4 | 3.298 | 259 | 126.1 | 1.869 |
| 26 | -3.3 | 215.284 | 65 | 18.3 | 72.513 | 104 | 40.0 | 28.393 | 143 | 61.7 | 12.552 | 182 | 83.3 | 6.128 | 221 | 105.0 | 3.248 | 260 | 126.7 | 1.844 |
| 27 | -2.8 | 208.905 | 66 | 18.9 | 70.667 | 105 | 40.6 | 27.766 | 144 | 62.2 | 12.309 | 183 | 83.9 | 6.023 | 222 | 105.6 | 3.198 | 261 | 127.2 | 1.819 |
| 28 | -2.2 | 202.739 | 67 | 19.4 | 68.876 | 106 | 41.1 | 27.155 | 145 | 62.8 | 12.072 | 184 | 84.4 | 5.921 | 223 | 106.1 | 3.150 | 262 | 127.8 | 1.794 |
| 29 | -1.7 | 196.780 | 68 | 20.0 | 67.136 | 107 | 41.7 | 26.559 | 146 | 63.3 | 11.840 | 185 | 85.0 | 5.820 | 224 | 106.7 | 3.102 | 263 | 128.3 | 1.770 |
| 30 | -1.1 | 191.019 | 69 | 20.6 | 65.447 | 108 | 42.2 | 25.979 | 147 | 63.9 | 11.613 | 186 | 85.6 | 5.721 | 225 | 107.2 | 3.056 | 264 | 128.9 | 1.746 |
| 31 | -0.6 | 185.449 | 70 | 21.1 | 63.806 | 109 | 42.8 | 25.413 | 148 | 64.4 | 11.391 | 187 | 86.1 | 5.625 | 226 | 107.8 | 3.010 | 265 | 129.4 | 1.722 |
| 32 | 0.0 | 180.063 | 71 | 21.7 | 62.212 | 110 | 43.3 | 24.861 | 149 | 65.0 | 11.174 | 188 | 86.7 | 5.530 | 227 | 108.3 | 2.965 | 266 | 130.0 | 1.699 |
| 33 | 0.6 | 174.855 | 72 | 22.2 | 60.664 | 111 | 43.9 | 24.323 | 150 | 65.6 | 10.962 | 189 | 87.2 | 5.437 | 228 | 108.9 | 2.920 | 267 | 130.6 | 1.677 |
| 34 | 1.1 | 169.817 | 73 | 22.8 | 59.160 | 112 | 44.4 | 23.799 | 151 | 66.1 | 10.755 | 190 | 87.8 | 5.346 | 229 | 109.4 | 2.877 | 268 | 131.1 | 1.654 |
| 35 | 1.7 | 164.944 | 74 | 23.3 | 57.698 | 113 | 45.0 | 23.288 | 152 | 66.7 | 10.552 | 191 | 88.3 | 5.257 | 230 | 110.0 | 2.834 | 269 | 131.7 | 1.632 |
| 36 | 2.2 | 160.230 | 75 | 23.9 | 56.278 | 114 | 45.6 | 22.789 | 153 | 67.2 | 10.354 | 192 | 88.9 | 5.170 | 231 | 110.6 | 2.792 | 270 | 132.2 | 1.610 |
| 37 | 2.8 | 155.669 | 76 | 24.4 | 54.899 | 115 | 46.1 | 22.303 | 154 | 67.8 | 10.160 | 193 | 89.4 | 5.084 | 232 | 111.1 | 2.751 | |||
| 38 | 3.3 | 151.255 | 77 | 25.0 | 53.557 | 116 | 46.7 | 21.828 | 155 | 68.3 | 9.970 | 194 | 90.0 | 5.000 | 233 | 111.7 | 2.710 | |||
| 40 | 4.4 | 142.848 | 81 | 27.2 | 48.557 | 122 | 50.0 | 19.217 | 163 | 72.8 | 8.593 | 204 | 95.6 | 4.244 | 245 | 118.3 | 2.276 |
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.