- Gas pressure switch may need to be adjusted: SZVAV application Min Supply Fan speed may also need to be raised in order to make switch.
- Diagnostics that may occur.
- These are seen at the Ignition Module
-
Factory setting is .25
Switch is adjustable from .15 To 4.0 IWC./Spanner Wrench Needed .
- Below is location of the Switch in the Burner section. Left Corner.
-
IPAK 3
Gas Heat Airflow Switch - Adjustment
Intellipak Symbio Combustion Fan proving switch
Articles in this section
- RAUJ, Voyager and IntelliPak Control Panel Labels
- How do you process a field modification request?
- TR150 & TR200 VFD Static Check Procedure
- What tool do I use to remove CoreMax Schrader Valves?
- How do you setup a Touch Screen Programmable Zone Sensor for use with a remote sensor?
- Intellipak Symbio Combustion Fan proving switch
- Symbio 800 Startup and Installation How-to Videos
- Danfoss TR Series Drive Literature
- Flow sensor failure. Pressure transducer troubleshooting
- Symbio 800 - Supply Air Pressure Calibration Solenoid.