Error Code H9: Pb error occurs 6 times within 120 minutes
Possible Causes
- The speed of the DC motor is abnormal
- Outdoor DC motor fault
- Communication fault between DC Fan Module board and Main board.
Troubleshooting
- If H9 occurs 6 times within 120 minutes. Refer to this link - Medium Foundation - Error Code Pb - Outdoor DC motor module protection – Trane Commercial HVAC Help Center
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.