Equipment
Overview
The system consists of an Odyssey A2L condenser equipped with Symbio 700 controls and an Odyssey A2L air handling unit (AHU) equipped with Symbio control boards. The AHU is configured with model number digit 15 = D, identifying the applicable unit configuration for this installation.
This equipment arrangement provides an integrated Odyssey A2L system with Modbus communication established between the condenser and AHU to enable coordinated control and system operation.
Wiring Info
How many wires do I need?
1 = Up to 7-conductor thermostat wire between the thermostat OR zone sensor and condenser
1 = Up to 6-conductor control wire between the AHU and condenser
2 = 2-conductor twisted, shielded, stranded communication wires between the AHU and condenser.
Recommended Communication Wire
Wiring Explanation
Cable Identification
AHU Wiring to Condenser - Cable #1 Modbus Communication
Cable #1 is a Modbus communication link between Symbio 700 and the AHU VFD. It is required for Pairing B as the AHU uses a communicating VFD. This cable must be a 2-conductor, twisted, shielded, stranded cable intended for 2 wire communications. We recommend Trane Purple Comm wire (Windy City Wire Spec #0523003) or any 2 conductor comm wire. 3 Conductor comm wire is also acceptable for Cable #1. Symbio Communication Wire
***DO NOT USE THERMOSTAT, ETHERNET OR NON-COMMUNICATION RATED WIRE FOR COMMUNICATIONS***
|
AHU Wiring to Condenser Cable #1 Modbus Communication | ||||||
|---|---|---|---|---|---|---|
|
AHU |
to |
Condenser |
|
||
| Cable | Board | Terminal | Board | Terminal | Description | |
| 1 | Relay Board | J7-1 | Adapter Board | J16-1 | Modbus + Communications for VFD | |
| Relay Board | J7-2 | Adapter Board | J16-2 | Modbus + Communications for VFD | ||
| Relay Board | J7-3 | Adapter Board | J16-3 | Comm drain (shield) wire, taped to back at AHU, do not connect at Relay board | ||
AHU Wiring to Condenser - Cable #2 Control Wiring
| AHU Wiring to Condenser Cable #2 Control Wiring | ||||||
|---|---|---|---|---|---|---|
AHU |
|
to |
Condenser |
|||
| Cable | Board | Terminal | Board | Terminal | Description | |
| 2 | Relay Board | J10-1 | Adapter Board | J15-1 | 24vac to power Relay Board | |
| Relay Board | J10-2 | Adapter Board | J15-2 | Comm/Neutral for Relay Board | ||
| Relay Board | J5-1 | Symbio 700 | J16-2 | Evap coil frostat, compressor shutdown | ||
| Relay Board | J5-4 | Adapter Board | J18-1 | Fan interlock for electric heat operation | ||
| Relay Board | J14-3 | Terminal Block | T2 | Refrigerant Sensor Alarm Contacts | ||
| Relay Board | J14-4 | Terminal Block | T1 | 24vac to Refrigerant Sensor Alarm Contacts | ||
| N/A | Relay Board | J10-1 | Relay Board | J4-1 | 24vac to IMC link, power for Indoor OM | |
| Relay Board | J10-2 | Relay Board | J4-2 | 24 neutral/common to IMC link, power for Indoor OM | ||
AHU Wiring to Condenser - Cable #3 IMC Communications
Cable #3 is an IMC communication link between Symbio 700 and the Indoor Option Module. It is required for electric heat operation and VVZT configuration. This cable must be a 2-conductor, twisted, shielded, stranded cable intended for 2 wire communications. We recommend Trane Purple Comm wire (Windy City Wire Spec #0523003) or any 2 conductor comm wire. Symbio Communication Wire
***DO NOT USE THERMOSTAT, ETHERNET OR NON-COMMUINCATION RATED WIRE FOR COMMUNICATIONS***
| AHU Wiring to Condenser Cable #3 IMC Communication | ||||||
|---|---|---|---|---|---|---|
AHU |
to |
Condenser | ||||
| Cable | Board | Terminal | Board | Terminal | Description | |
| 3 | Relay Board | J4-3 | Adapter Board | J15-3 | IMC + Communications for Indoor OM | |
| Relay Board | J4-4 | Adapter Board | J15-4 | IMC + Communications for Indoor OM | ||
| Adapter Board | J15-2 | Comm drain (shield) wire, taped back at AHU, do not connect at Relay Board | ||||
Wiring Thermostat to Condenser - Cable #4A Thermostat Wiring
Cable #4A is for conventional thermostat use or when the condenser is controlled by relays. Unit will only use Cable #4A or 4B, not both.
| Condenser to Thermostat Cable #4 Thermostat Wiring | ||||||
|---|---|---|---|---|---|---|
|
Condenser |
|
to |
Thermostat |
|
|
| Cable | Board | Terminal | Board | Terminal | Description | |
| 4 | Symbio 700 | J21-1 (24vac) | Thermostat | R | 24vac | |
| Symbio 700 | J21-2 (Y1) | Thermostat | Y1 | Cool 1 (Heat call on Heat Pump) | ||
| Symbio 700 | J21-3 (W1/O) | Thermostat | W1 or O/B | Heat 1 (reversing valve call on Heat Pump) | ||
| Symbio 700 | J21-4 (G) | Thermostat | G | Fan | ||
| Symbio 700 | J21-5 (W2) | Thermostat | W2 | Heat 2 (Aux heat on Heat Pump) | ||
| Symbio 700 | J21-6 (Y2) | Thermostat | Y2 | Cool 2 (Heat call on Heat Pump) | ||
| Symbio 700 | J21-7(X2) | Thermostat | Aux | Emergency Heat on Heat Pump (will shut down compressors) | ||
| Symbio 700 | J21-8 (T) | Thermostat | Pulldown | Heat Anticipator/Pulldown (not commonly used) | ||
| Symbio 700 | J21-9 (Com) | Thermostat | Comm | Common/Neutral for Thermostat | ||
Wiring Zone Sensor to Condenser - Cable #4B Thermostat Wiring
Cable #4B is for zone sensor use and required when VVZT (SZVAV) operation is desired. Zone sensors are commonly used with BAS or can be standalone. Unit will only use Cable #4A or 4B, not both.
| Condenser to Zone Sensor Cable #4 Zone Sensor Wiring | ||||||
|---|---|---|---|---|---|---|
|
Condenser |
to |
Zone Sensor |
|
||
| Cable | Board | Terminal | Board | Terminal | Description | |
| 4 | Symbio 700 | J19-1 | Zone Sensor | 1 | Zone Temp | |
| Symbio 700 | J19-2 | Zone Sensor | 2 | Common | ||
| Symbio 700 | J19-3 | Zone Sensor | 3 | Cooling Setpoint | ||
| Symbio 700 | J19-4 | Zone Sensor | 4 | Unit Mode & Fan Speed (Fan Speed not supported on all units) | ||
| Symbio 700 | J19-5 | Zone Sensor | 5 | Heating Setpoint | ||
| Symbio 700 | J19-6 | Zone Sensor | Ground | Common/Neutral for 24vac | ||
| Symbio 700 | J19-7 | Zone Sensor | 24vac | 24vac | ||
*Zone sensor wiring shown for BAYSENS135, other mechanical zone sensors similar.
Emergency Stop Wiring - From Stop Devices to Symbio 700
| Emergency Stop Wiring From Stop Devices to Symbio 700 | ||||||
|---|---|---|---|---|---|---|
|
AHU |
to |
Condenser |
|
||
| Cable | Board | Terminal | Board | Terminal | Description | |
| N/A | Stop Device | Common | Symbio 700 | J18-1 | 24vac Out to Stop Device(s) | |
| Stop Device | Norm. Closed | Symbio 700 | J18-2 | 24vac Input from Stop Device(s) | ||
The wiring above reflects normally closed safeties. Typically, condensate overflow switches (or pan switches) are normally closed devices. If using normally open devices, they can be wired in parallel, and the Customer Connection Polarity does not need to be changed.
For more information see the links below:
- Trane Commercial Help Center - Symbio™ 700 - Emergency Stop Input
- Trane Commercial Help Center - Symbio 700 Demand Limit and Emergency Stop Polarity
Configuration
Configuring the Symbio 700
Odyssey condensers can be paired with many different Odyssey AHUs, 3rd party AHUs, and indoor coil assemblies. Due to this, Symbio 700 must be configured for the connected AHU, installed accessories, and controlling sensor/thermostat.
Here is an article on accessing and editing the Configuration through the Mobile Phone App:
For Variable Volume Zone Temperature (VVZT or formerly known as SZVAV) operation, set the configuration as follows:
System Type = VVZT (requires zone sensor for actual VVZT operation, conventional thermostat will operate as CVZT)
Efficiency = Standard B
Indoor Fan Type = Variable Speed (should set automatically)
-
Space Controller = Conventional Thermostat, Single Setpoint Zone Sensor, or Dual Setpoint Zone Sensor
Zone Sensor will use DAT logic for compressor staging
Frostat = Installed (should install automatically)
Discharge Temperature Sensor = Installed (should install automatically)
-
Field installed electric heat only
-
TTA condenser
Primary Heating Source = Electric
Primary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TWA condenser
Secondary Heating Source = Electric
Secondary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
For Multispeed fan operation, set the configuration as follows:
System Type = CVZT (thermostat or zone sensor)
Efficiency = Standard B
Indoor Fan Type = Multi Speed
Space Controller = Conventional Thermostat, Single Setpoint Zone Sensor, Dual Setpoint Zone Sensor
Frostat = Installed
-
Discharge Temperature Sensor = Installed or Not Installed
Not required for operation, but it is already installed in the air handler.
Zone Sensor will use DAT logic for compressor staging.
-
Field installed electric heat only
-
TTA condenser
Primary Heating Source = Electric
Primary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TWA condenser
Secondary Heating Source = Electric
Secondary Heating Stages = 1 or 2 (depending on electric heat kit stages
-
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.