- BCI-R will not go into BAS control. Always remains in Standalone control.
- Unit cannot be controlled by the zone sensor.
- Unit cannot be controlled by the thermostat.
Process (Steps 1-7):
- Configure TD5 Local Display for System Control ("Read Mode"):
- If the Auto and Stop buttons are displayed in the top right hand corner then the TD5 is in Write mode.
Access the Settings menu by tapping Settings.
Image 1. Main Menu - Write Mode
Tap on the Setup button once the Settings menu is open.
Image 2. Settings Menu
- Tap on the Display Read Only Mode button to change from Write mode to Read Only mode.
Tap the Save button (not shown).
Image 3. Setup Menu
Once the Read Only mode has been established the Auto and Stop buttons will no longer be shown on the Main menu.
Image 4. Main Menu - Read Only Mode
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.