Using a BAYSENS108 and a BAYSENS077 as an example.
- The BAYSENS077 will report the temperature back to the Symbio 700 while the BAYSENS108 can still control the setpoint and mode.
- For example, the BAYSENS077 can be located in a lobby while the BAYSENS108 can be installed in a secured area to prevent tampering.
- If the BAYSENS077 is used without the BAYSENS108, the Symbio 700 will default to a 70 degree heating setpoint and 75 degree cooling setpoint. The mode will be in auto with the supply fan on.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.