Wiring
The terminal connections between the Gen 2 and Gen 3 EBMPapst fans are not the same. The pin correlation below needs to be used when replacing a Gen 2 fan with a Gen 3 fan. The replacement Gen 3 fan will not have a wiring harness, the original harness from the Gen 2 fan will need to be reused.
Equipment
6-10T ReliaTel Precedent units with Gen 2 EBM Papst Supply Fan (pre 2017)
- T/YSC072-120F
- T/YHC072-120F
- When replacing FAN04214 or FAN04605 with FAN07046 (208-230vac)
- When replacing FAN04215 or FAN04606 with FAN07045 (460/575 vac)
Use the pin correlation below when replacing a Gen 2 fan with a Gen 3 fan to ensure the correct terminations.
Wiring harnesses
Mounting
Certain older Precedent models equipped with the Gen 2 motor feature an 8-bolt pattern. The motor mount in the frame may not correspond to the correct bolt pattern for the new motor, which utilizes a 6-bolt pattern. This is seen primarily on the early launch Precedent models with the Gen 2 motors ~2011-2012/13.
There are 2 options when dealing with this issue:
- Two of the mounting holes will line up between the 8-bolt and 6-bolt, line up these 2 holes and drill out the other 4
Order PLT06399 which include both bolt patterns
click to enlarge click to enlarge
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.