A BACnet-compliant Thermostat is currently offered through the Controls Group as a possible solution to using Electromechanical Precedents, Foundation units, or when a BACnet retrofit is being conducted on older Voyager II UCP (with a CTI) micro-controlled units. These thermostats will output a 24vac signal when communicated to do so by BACnet. The ability to wire three individual sensors (10kOhm at 77 degrees) and two switches back to these thermostats is possible for readout at the front end system.
24-volt BACnet thermostat - User Guide (attached below)
Thermostats -
TSTAT BACnet, RTU 3H2C - X13511541010 / Part #THT02988
TSTAT BACnet, RTU HP - X13511542010 / Part #THT02980
NOTE: Always check for the latest documentation
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.