This pairing and wiring is used when the air handler ordered is not setup for communication, but communication wire is needed for the application. This application may be BAS control, zone sensor control, SZVAV control, or Symbio full functionality, for some examples. The VFD will need to be reprogrammed, and a Modbus communication wire installed directly to the VFD essentially modifying the unit close to an air handler (15th digit = D).
Symbio 700 Quick Links
- Symbio™ 700 - Where to download the Service & Installation Mobile Phone App
- Symbio™ 700 - Bluetooth Connection Instructions
- Symbio™ 700 - Precedent or Odyssey - How to configure or edit configurations using the Mobile Phone App
Equipment
- Condenser: Odyssey A2L Condenser with Symbio 700 controls
- Air Handler: Odyssey A2L AHU with Symbio control boards and model number digit 15 = C
Field Wiring
How many wires do I need?
- 1 - Up to 7 conductor thermostat wire between the thermostat OR zone sensor and condenser
- 1 - Up to 6 conductor control wire between the AHU and condenser
- 2 - 2-conductor twisted, shielded, stranded communication wires between the AHU and condenser.
Cable Identification
AHU Wiring to Condenser
Cable #1 Modbus Communication
Cable #1 Modbus Communication
Cable #1 is a Modbus communication link between Symbio 700 and the AHU VFD. It is required for Pairing B as the AHU uses a communicating VFD. This cable must be a 2-conductor, twisted, shielded, stranded cable intended for 2 wire communications. We recommend Trane Purple Comm wire (Windy City Wire Spec #0523003) or any 2 conductor comm wire. 3 Conductor comm wire is also acceptable for Cable #1. Symbio Communication Wire
| AHU | to | Condenser | ||||
|---|---|---|---|---|---|---|
| Cable | Board | Terminal | Board | Terminal | Description | |
1 |
TR150 VFD | 68 | Adapter Board | J16-1 | Modbus + Communications for VFD | |
| TR150 VFD | 69 | Adapter Board | J16-2 | Modbus - Communications for VFD | ||
| Adapter Board | J16-3 | Comm drain (shield) wire, taped back at AHU, do not connect at Relay Board | ||||
Cable #2 Control Wiring
Cable #2 Control Wiring
| AHU | to | Condenser | ||||
|---|---|---|---|---|---|---|
| Cable | Board | Terminal | Board | Terminal | Description | |
2 |
Relay Board | J10-1 | Adapter Board | J15-1 | 24vac to power Relay Board | |
| Relay Board | J10-2 | Adapter Board | J15-2 | Comm/Neutral for Relay Board | ||
| Relay Board | J5-1 | Symbio 700 | J16-2 | Evap coil frostat, compressor shutdown | ||
| Relay Board | J5-4 | Adapter Board | J18-1 | Fan interlock for electric heat operation | ||
| Relay Board | J14-3 | Terminal Block | T2 | Refrigerant Sensor Alarm Contacts | ||
| Relay Board | J14-4 | Terminal Block | T1 | 24vac to Refrigerant Sensor Alarm Contacts | ||
| N/A | Relay Board | J10-1 | Adapter Board | J4-1 | 24vac to IMC link, power for indoor OM | |
| Relay Board | J10-2 | Adapter Board | J4-2 | 24 neutral/comon to IMC link, power for Indoor Om | ||
Cable #3 IMC Communication
Cable #3 IMC Communication
(Only required when an Indoor Options Module is installed)
Cable #3 is an IMC communication link between Symbio 700 and the Indoor Option Module. It is required for electric heat operation and VVZT configuration. This cable must be a 2-conductor, twisted, shielded, stranded cable intended for 2 wire communications. We recommend Trane Purple Comm wire (Windy City Wire Spec #0523003) or any 2 conductor comm wire. Symbio Communication Wire
| AHU | to | Condenser | ||||
|---|---|---|---|---|---|---|
| Cable | Board | Terminal | Board | Terminal | Description | |
3 |
Relay Board | J4-3 | Adapter Board | J15-3 | IMC + Communications for Indoor OM | |
| Relay Board | J4-4 | Adapter Board | J15-4 | IMC - Communications for Indoor OM | ||
| Symbio 700 | J15-2 | Comm drain (shield) wire, taped back at AHU, do not connect at Relay Board | ||||
Condenser to Thermostat
Cable #4 Thermostat Wiring
Cable #4 Thermostat Wiring
| Condenser | to | Thermostat | ||||
|---|---|---|---|---|---|---|
| Cable | Board | Terminal | Board | Terminal | Description | |
| 4|A | Symbio 700 | J21-1 (24vac) | Tstat | R | 24vac | |
| Symbio 700 | J21-2 (Y1) | Tstat | Y1 | Cool1 (Heat call on Heat Pump) | ||
| Symbio 700 | J21-3 (W1/O) | Tstat | W1 or O/B | Heat1 (reversing valve call on Heat Pump) | ||
| Symbio 700 | J21-4 (G) | Tstat | G | Fan | ||
| Symbio 700 | J21-5 (W2) | Tstat | W2 | Heat2 (Aux heat on Heat Pump) | ||
| Symbio 700 | J21-6 (Y2) | Tstat | Y2 | Cool2 | ||
| Symbio 700 | J21-7 (X2) | Tstat | Aux | Emergency Heat on Heat Pump (will shut down compressors) | ||
| Symbio 700 | J21-8 (T) | Tstat | Pulldown | Heat Anticipator/Pulldown (not commonly used) | ||
| Symbio 700 | J21-9 (Comm) | Tstat | Comm | Common/Neutral for tstat | ||
Cable #4 Zone Sensor Wiring
Cable #4 Zone Sensor Wiring
| Condenser | to | Zone Sensor | ||||
|---|---|---|---|---|---|---|
| Cable | Board | Terminal | Board | Terminal | Description | |
| 4B | Symbio 700 | J19-1 | Zone Sensor | 1 | Zone Temperature | |
| Symbio 700 | J19-2 | Zone Sensor | 2 | Common | ||
| Symbio 700 | J10-3 | Zone Sensor | 3 | Cooling Setpoint | ||
| Symbio 700 | J19-4 | Zone Sensor | 4 | Unit Mode | ||
| Symbio 700 | J19-5 | Zone Sensor | 5 | Heating Setpoint | ||
| Symbio 700 | J19-6 | Zone Sensor | 6 | Common | ||
| Symbio 700 | J19-7 | Zone Sensor | 7 | 24 vac | ||
*Zone sensor wiring shown for BAYSENS135, other mechanical zone sensors are similar.
Emergency Stop Wiring
From Stop Devices to Symbio 700
From Stop Devices to Symbio 700
| Stop Device | to | Condenser | ||||
|---|---|---|---|---|---|---|
| Cable | Board | Terminal | Board | Terminal | Description | |
| N/A | Stop Device | Common | Symbio 700 | J18-1 | 24vac Out to Stop Devices | |
| Stop Device | Norm. Closed | Adapter Board | J18-2 | 24vac Input from Stop Devices | ||
Wiring above reflects normally closed safeties. Typically, condensate overflow switches (or pan switches) are normally closed devices. If using normally open devices, they can be wired in parallel, and the Customer Connection Polarity does not need to be changed.
For more information see the links below:
- Trane Commercial Help Center - Symbio™ 700 - Emergency Stop Input
- Trane Commercial Help Center - Symbio 700 Demand Limit and Emergency Stop Polarity
Configuring the Symbio 700
Odyssey condensers can be paired with many different Odyssey AHUs, 3rd party AHUs and indoor coil assemblies. Due to this, Symbio 700 must be configured for the connected AHU, installed accessories, and controlling sensor/thermostat.
Here is an article on accessing and editing the Configuration through the Mobile Phone App:
For Variable Volume Zone Temperature (VVZT or formerly known as SZVAV) operation, set the configuration as follows:
- System Type = VVZT (requires zone sensor for actual VVZT operation, conventional thermostat will operate as CVZT)
- Efficiency = Standard B
- Indoor Fan Type = Variable Speed (should set automatically)
- Space Controller = Conventional Thermostat, Single Setpoint Zone sensor, or Dual Setpoint Zone Sensor (zone sensor will use DAT logic for compressor staging)
- Frostat = Installed (should install automatically)
- Discharge Temperature Sensor = Installed (should install automatically)
-
Field installed electric heat only
-
TTA condenser
- Primary Heating Source = Electric
- Primary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TWA condenser
- Secondary Heating Source = Electric
- Secondary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TTA condenser
For Multispeed fan operation, set the configuration as follows:
- System Type = CVZT (thermostat or zone sensor)
- Efficiency = Standard B
- Indoor Fan Type = Multi Speed
- Space Controller = Conventional Thermostat, Single Setpoint Zone sensor, or Dual Setpoint Zone Sensor
- Frostat = Installed
- Discharge Temperature Sensor = Installed (Not required for operation, but it is already installed in the air handler. Zone Sensor will use DAT logic for compressor staging) or Not Installed
-
Field installed electric heat only
-
TTA condenser
- Primary Heating Source = Electric
- Primary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TWA condenser
- Secondary Heating Source = Electric
- Secondary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TTA condenser
VFD programming
If assistance is needed in programming the VFD, here is an article to help:
Confirm or change the following parameters in the TR150 VFD:
- Change 3-15 from [1] Analog Input 53 to [11] Local Bus Reference.
- Change 5-10 from [8] Start to [0] No Operation
- Change 8-01 from [0] Digital and Control Word to [2] Control Word Only
- Change 8-03 to [15] 15 seconds
- Change 8-04 to [2] Stop
- Change 8-30 to [2] Modbus RTU
- Change 8-31 to [2] Address 2
- Change 8-32 to [7] 115200 Baud
- Change 8-33 to [0] Even Parity, 1 Stop Bits
- Change 8-35 to [0.005] 5ms Min Response Delay Time
- Change 8-36 to [0.1] 100mx Max Response Delay Time
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.