Temporary comfort can be provided without a zone sensor module or thermostat in place by using the outdoor air sensor or a spare supply air/return air sensor. How to do it: remove the sensor from the unit, add enough thermostat wire to it so that it can be placed in the return air stream, then connect the sensor to J6-1 & J6-2.
After the permanent zone sensor or thermostat is in place, the sensor must be removed from J6-1 & J6-2. If the RTRM does not have a space temperature input (J6-1, J6-2), or has a conventional thermostat input (G, Y, W), the unit will not run (except in the test mode).
Temporary Sensor (Thermistor)
Attached to J6-1 and J6-2 Only
- Continuous fan
- Auto changeover
- 74°F cooling, 71°F heating
- Note: 27.5 to 50 tons - the outdoor air sensor should not be used for this purpose.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.