To clear BCI2-R using the embedded service tool and rebuilding the points, you can follow the general steps:
1. Power unit off and connect USB cable to controller USB will power the controller to do this process. Open web browser and type in address 198.80.18.1.
2. Click onto Login.
- Verify the points which outputs are in service to be able to put them in service after clearing contoller
- Verify the bacnet information in identification and communication
3. Once clicking onto the login the screen will show Fig. 2 Click on tools.
4. Once in tools click onto Backup and Restore.
5. Click on Clear controller.
6. Click on confirm
7. A window will appear Success click on Ok to continue
8. End User License Agreement
- Click on Yes.
- Click on Continue.
- Once that is done it will revert back to Fig. 2
- Disconnect from the controller wait 30 seconds.
Power unit up and wait 5 minutes for the controller to pull the points back into the controller before connecting with the USB cable.
9. Trane Tracer SC+ only
If installed on a Tracer SC+ it may be necessary to refresh the equipment.
- In Synchrony select the Devices tab
- Check the checkbox next to the device
- From the actions tab at the top of the list select Refresh
- If the refresh fails, the BCI2 BACnet address has probably changed. This can be addressed by selecting Replace instead of Refresh and discovering the Link that the controller is connected to. Follow the prompts until complete.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.