Low oil flow?
The 70-125 ton RTXX chiller platform does NOT use an oil DP switch.
Verify the correct compressor model number is selected in Service Settings \ Machine Configuration, this should be CHHN for these chillers.
RTAA 70-125 TON, RTWA 70-125 TON, RTUA 70-125 TON chillers.
On the compressor module for each circuit, verify there is a good electrical connection on the jumper wired between J3-1 to J3-2. See example below of Circuit 2 (1U5) DP Switch Input Jumper.
Notes
- Additional information see Oil Flow Control Diagnostic?
- In addition it is advised to check the other settings/setpoints in Machine Configuration and Service Setup Menu's.
See appropriate IOM for reference.
Additional details
Other Question/Problem/Cause Statements
- Low oil flow?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Compressor Chiller (Pueblo) (RTUA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.