COMP CONTACTOR FAIL (CKT1 or CKT2)
This diagnostic occurs if compressor proving input(s) on the SCM/MCM (1U49) does not open within three seconds of the call for lead compressor on a circuit to stop or the input is closed when all compressors on a circuit should be off.
- The unit controls assume that the compressor contactor has welded closed.
- The input on the SCM/MCM (1U49) is connected to the normally open contacts of an auxiliary switch on the side of the lead compressor contactor on each circuit.
- This is a manual reset diagnostic.
Items to check include:
- unit wiring,
- switch operation/bad contactor,
- control module
Here are the steps for Intellipak Air-Cooled Chiller
- Wiring Error
- Verify the wiring between the compressor auxiliary switch and the SCM (1U49 on 20-30 ton units) or the MCM (1U49 on 40-60 ton units).
- Also verify the wiring of the compressor contactor coil circuit. Refer to unit schematics for wire numbers and connections.
- If the wiring checks good, continue to the next step.
- Switch/Contactor Checkout
- Disconnect power from the unit.
- Verify compressor contactor is open. With an ohmmeter, verify auxiliary contacts are also open.
- If no problems are found, continue to the next step.
- Control Module
- If no problems are found in the above steps, the proving input on the SCM/MCM (1U49) may not be functioning.
- Reset the unit diagnostic and place a jumper on that input.
- If Compressor Contactor Failure diagnostic appears, the input/board is good.
- If not, replace the SCM/MCM (1U49).
Additional details
Facts
- Intellipak Air-Cooled Chiller 20-60
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.