LIQUID PRESSURE SENSOR FAILURE (CKT-1/CKT-2)
This diagnostic occurs when there is not a valid signal on the liquid pressure sensor input on the SSM (1U91).
- The sensor has an operational range of 0 to 5 VDC.
- These sensors would only exist on IntelliPak chiller units with the Superheat/Subcooling option installed and are located on the liquid line of each refrigeration circuit (designated as 4U92 for circuit 1 and 4U94 for circuit 2).
- This is an information only diagnostic and will clear automatically when the module measures a valid voltage.
- This diagnostic will not affect the operation of the unit.
Here are the steps for Intellipak Air-Cooled Chiller
- Sensor Calibration Setting
- Verify the calibration setting in the pressure transducer device characteristics located in the Setup Menu.
- For Liquid Pressure Sensors, the settings should be: 0 PSIG = 0.118 VDC & 400 PSIG = 4.847 VDC.
- The Ckt1 Liquid Line Pressure Transducer setup screen appears only if the Superheat/Subcooling option is installed. This screen allows the user to adjust the voltage to pressure calibration setpoints at 0 PSIG (0.000 - 4.000 VDC) and 100 PSIG (1.000 - 5.000 VDC).
- Ckt 1 Liquid Line Pressure Transducer
- 0 PSIG = 0.118 VDC
- 100 PSIG = 4.847 VDCThe Ckt2 Liquid Line Pressure Transducer setup screen appears only on 40-60 Ton units with the Superheat/Subcooling option installed. This screen allows the user to adjust the voltage to pressure calibration setpoints at 0 PSIG (0.000 - 4.000 VDC) and 100 PSIG (1.000 - 5.000 VDC).
- Ckt 2 Liquid Line Pressure Transducer
- 0 PSIG = 0.118 VDC
- 100 PSIG = 4.847 VDC
- Ckt 1 Liquid Line Pressure Transducer
- Wiring Error
- Verify the wiring between the Liquid Pressure Sensor and the SSM (1U91).
- Refer to unit schematics for wire numbers and connections.
- If the wiring checks good, proceed to the next step.
- Sensor Checkout
- The sensors used to determine liquid pressure are 3 wire pressure transducers.
- These transducers require an operating supply voltage of 4.5 ? 5.5 VDC. Verify the supply voltage from the SSM (1U91).
- If the voltage is not in this range, disconnect the plug connector from the SSM (1U91) and verify proper supply voltage.
- If supply voltage is not present, replace the SSM (1U91).
- Once supply voltage has been confirmed, re-connect the plug connector and check the output voltage of the pressure transducer.
- Convert this voltage to a pressure based on the linear scale 0 PSIG (@ 0.118 VDC) to 400 PSIG (@4.847 VDC).
- If the output is not correct versus an actual pressure gauge reading, replace the pressure transducer.
- If the output is not correct versus the HI display of liquid pressure, replace the SSM (1U91).
Additional details
Facts
- Intellipak Air-Cooled Chiller 20-60
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.