The best way to repair leaks on the drive cooling fluid system
The RTAE chiller utilizes a cooling fluid system for the AFD3 (and load inductors for initial release RTAE Chillers). The system consists of circulation pump, Braze Plate Heat Exchanger and a bypass cooling circuit.
For mechanical threaded joints in is recommended to use a thread sealant such as Loctite 561 PST Pipe Sealant (used in the Trane factory where RTAE is built). DO NOT use Teflon tape for any joints.
Hose clamps are used for all hose to fitting connections. For leaks in these areas, it may be necessary to tighten or replace the coupling at that particular joint.
Trane Heat Transfer Fluid part number: CHM01023
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.