This diagnostic means that the unit mounted Human Interface (HI , 1U65) is not communicating with Cold Generator Module (CGM, 1U48). The cause for this can be as follows:
- wiring error
- defective HI
- defective module other than HI
- All the modules share a comm link using twisted wire.
- The J1 connector on each module is the connection point for this comm link.
- They all connect to a common point on the 1TB9 terminal strip mounted over the CGM.
- The comm link is polarity sensitive.
Here are the steps for Intellipak Air-Cooled Chiller
- Wiring Error
- Verify proper wiring between HI to 1TB9 and CGM to 1TB9.
- Refer to unit wiring diagram control box door for wire numbers and connection points.
- Check for good connections and proper polarity.
- If no errors are found, proceed to Step 2.
- Defective Human Interface
- There is no way to check the Human Interface other than take it to a known good unit and test it.
- If the HI does not function in a known good unit, replace it.
- As a note, a defective HI will not prevent the unit from functioning normally in other aspects.
- So, if the unit is operating properly, it is a good indication that the HI is defective.
- If the HI functions in another unit or the unit is not functioning, proceed to Step 3.
- Module Problems
- If the CGM (1U48) does not have 24 VAC, this diagnostic will be generated.
- Check for 24 VAC at J2 on the CGM.
- If 24 VAC is not present, check wiring.
- Refer to unit schematics on the control box door.
- If 24 VAC is present at J2, continue below.\
- Disconnect unit power.
- Unplug the J1 and J2 connectors from all modules except the HI and the CGM.
- Restore power to the unit.
- If communications are restored, one of the modules has a problem.
- Plug them back up, one at a time, to find which one is pulling the comm link down.
- Check that module for wiring errors per the unit schematics.
- If none are found replace that module.
- If communications are not restored, continue below.
- Disconnect unit power.
- Unplug all connectors except J1 and J2 on the CGM.
- If communications are restored, check module wiring per unit schematics.
- If communications are not restored, replace CGM.
- If possible verify defective CGM by exchanging with a CGM from another unit.
Additional details
Facts
- Intellipak Air-Cooled Chiller 20-60
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.