Check the phase to phase voltage and compare it to the nameplate voltage. It should be within +/- 10% of the nameplate voltage. Check that the menu settings for voltage are correct. Finally, check the under/over voltage transformer, 1T2. It should have a 20:1 ratio. Refer to service bulletin RTAA-SB-5 or RTAA-SVD03A-EN for further information.
Additional details
Resource Available
- Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- Service Guide: RTAA-SB-5, RTAA-SVD03A-EN
Other Question/Problem/Cause Statements
- Getting a d8 under voltage diagnostic.
- Under/over voltage trip.
- Getting d7 over voltage diagnostic.
Facts
- RTAA 130-400 TON (PUEBLO)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.