Oil Change
Trane does not recommend changing oil in Series R Chillers unless an oil analysis indicates a need to do so (such as in the case of a severe motor burnout).
See RTAA-SB-6A for further information on RTAA/WA/UA chillers and RTHA-SB-16 on RTHA/B chillers.
It is recommended that an annual oil analysis be performed by a qualified laboratory. The first reading can serve as a baseline, and subsequent tests should be used to trend moisture, acid, and wear metal levels.
Additional details
Other Question/Problem/Cause Statements
- Oil Change
Facts
- RTAA 130-400 Ton (Pueblo)
- RTAA 70-125 Ton (Pueblo)
- RTAC
- RTHA, RTHB
- RTHC (Pueblo)
- RTUA
- RTWA
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.