What is Low Ambient Lockout?
This is a user enabled feature that prevents a unit from starting whenever the ambient temperature is below a specific setpoint. The factory default of the feature is "Disabled", and the setpoint range is between -20 (20 below zero) and 40 F. The factory default is 20 F.
It comes standard on CGA, CGAF, CGAM, CCAF, RTUA, RTAA, RTAC, RTAF, RTAE, ACSA, and ACR units.
It is not available from the unit controller on the CGWF, RTWA, RTHB, RTWD, or RTHD. If a water-cooled unit is to be shut off based upon low ambient lockout temperature, then a separate thermostat/controller (wired to the external auto/stop switch) or BAS system must be used to shut the chiller off.
Additional details
Other Question/Problem/Cause Statements
- What is Low Ambient Lockout?
- Can the chiller be locked out on low ambient?
Facts
- Air-Cooled Chiller - Intellipak (CGAF)
- Air-Cooled Chiller (CGA, 10-15 Ton)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Condenser (Pueblo) (RTCA)
- Compressor Chiller (Pueblo) (CCAF)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Air-Cooled Chiller (Pueblo) (RTAF)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Air-Cooled Chiller (Pueblo) (ACR)
- Air-Cooled Chiller (Pueblo) (ACSA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.