The orifice plates under the male loader/unloader valves part numbers are:
- PLT03713 ( X05140386010) → 0.0325"
- PLT03712 ( X05140386020) → 0.0255"
The smaller orifice plate goes under the male load solenoid valve, and the larger orifice plate goes under the male unload solenoid valve.
See service bulletin RTAA-SVB12A-EN for additional information.
That plate is an orifice plate that must be kept for proper oil metering.
Additional details
Resource Available
-
Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- Service Guide: RTAA-SVB12A-EN
Other Question/Problem/Cause Statements
- Which orifice plate goes under the solenoid valves?
- Which orifice plate goes under the load solenoid valve?
- Which orifice plate goes under the unload solenoid valve?
- When replacing the male and female solenoid valves, there is a thin metal plate with a hole in it that is between the valve and compressor. Do this need to be kept or should it be gotten rid of like the pill filters?
- Does the orifice plate between the unloader solenoid valves need to be kept or can it be discarded?
- GP1 Male Loader/Unloader Orifice Plates
Facts
- RTAA 70-125 Ton (Pueblo)
- RTUA
- RTWA
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
- RTAA 70-125 TON (PUEBLO)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.