- Verify that all wiring is correct and tight.
- Attach a hose from the male piston schrader to suction and try to start the compressor unloaded.
- If unsuccessful at above, remove refrigerant from compressor and manually turn rotors to see if they are stuck or hanging up.
Additional details
Other Question/Problem/Cause Statements
- Compressor is tripping on overload.
- Chiller cannot fully ramp up and is tripping on current overload.
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.