An RTAA purchased for standard leaving water temperatures (60-40 deg F) can be converted to produce low leaving water temperatures (<40 deg F).
To convert the RTAA, the settings for the Low Evaporator Temperature Cutout and Low Water Temperature Cutout need to be adjusted. These setting can be referenced in the RTAA IOM's.
- For RTAA 130-400, use IOM RTAA-IOM-3 page 102.
- For RTAA 70-125, use IOM RTAA-SVX01A-EN page 97.
- The refrigerant piping between the RTUA and air-cooled condenser should be evaluated to ensure the piping is sized correctly for the lower LWT.
- This does not apply to the RTWA ordered at comfort cooling temperatures. For low temperature and high condenser applications, the compressors are different and an oil cooler may have to be installed.
It is best to contact the Trane Field Modifications Group in La Crosse. Non-Trane customers should contact their local Trane parts counter first and then the parts counter can contact the Field Modifications Group.
Additional details
Resource Available
- Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- IOM: RTAA-IOM-3 and RTAA-SVX01A-EN
Other Question/Problem/Cause Statements
- Converting RTAA from standard to low leaving water temperatures
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.