What can cause a motor burn?
Typical causes of a motor burn can be:
- Lightning strikes in the area of the chiller
- Poor electrical power provided to chiller, including brown outs and power surges
- Motor failure caused by a defect in the motor or damage to the motor during installation
- Debris in the compressor
- Water in the system
- Loose wire connections
- Excessive condensation on motor terminal plate
- Disabled motor protections
- High acidity level in refrigerant and oil
Additional details
Other Question/Problem/Cause Statements
- What can cause a motor burn?
- Causes of motor burnout
- Compressor motor failure
Facts
- RTHD
- Air-Cooled Chiller (Charmes) (RTAA)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Charmes) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.