Is it possible to disable the "B" compressor on circuit one on a three compressor chiller?
- Be sure the chiller switch is in the STOP/RESET position.
- Go into the UCM menu item 50 and change it from 3 compressors to 2.
- Remove power from the chiller.
- Remove fuse F1 from the 1U5 module.
- Re-apply power to the chiller.
- Change the address dip switch on the 1U6 module from 1=On, 2=Off to 1=Off, 2=On.
- If the compressors are different sizes, change menu item 56 current overload setting and the 1U6 dip switch settings to correspond with the compressor that is now running.
- Re-start the chiller.
Notes
- This procedure does NOT apply if compressor "1A" is down on a three compressor chiller.
Additional details
Other Question/Problem/Cause Statements
- Is it possible to disable the "B" compressor on circuit one on a three compressor chiller?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.