What can cause suction temperature too high on CGAM units?
- This diagnostic is generated when the suction temperature measurement is larger than the entering temperature threshold value for 5 continuous minutes.
- Check that the suction temperature sensor is installed in the well properly for the respective circuit.
- Check that there is adequate thermal paste.
- Verify temperature sensor temperature is indicating on the display versus thermocouple measured temperature
- Check that entering water temperature sensor is reading correctly
Notes
- Diagnostic 7148 is equivalent to the suction temperature too high alarm. Main Processor software in the Dynaview should be upgraded to reflect the verbiage of this code.
Additional details
Resource Available
-
Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- IOM: CG-SVX17N-EN
- Service Guide: CG-SVG002E-EN (Internal ONLY: Proprietary to Trane)
Other Question/Problem/Cause Statements
- What can cause suction temperature too high?
- Suction Temperature too high?
- Suction Temp?
- What can cause ?7148
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.