Phase loss diagnostics on compressor A and/or B
- Check wiring connections from starter to Current Transformers (CT's)
- Checkout Current Transformers (CTs) and check resistance across each one while it is disconnected. All resistances should be within 10% of one another.
- Also do a diode test on the CT inputs on each compressor module. (The diode test is described in RTAA-SVB10B-EN.)
- Check for a chattering or malfunctioning High Pressure Cutout (HPC). Use a jumper temporarily to see if problem goes away.
- Check for 120 volts at J7-3 on the compressor modules (1U4 or 1U5) when the compressor is trying to start.
- Check the 1K2 Aux 2 (RUN) contact and 1K4 Aux1 (TRANSITION) contact for compressor A and the 1K6 Aux 2 (RUN) and 1K8 Aux1 (TRANSITION) contacts for compressor B. These should be a dead short, normally closed contacts. If there is any amount of resistance, replace them.
- Check for any swapping of 115 volt and neutral wiring on the 1U4/1U5
Notes
- The diode test is described in RTAA-SVB10B-EN
Additional details
Resources Available
-
Reference Literature:
(Electronic copies can be pulled from e-library at Trane Residential) - IOM: RTAA-SVX01A-EN
- Troubleshooting Guide: RLC-SVD03A-EN
- Compressor Module Troubleshooting: RTAA-SVB10B-EN
Other Question/Problem/Cause Statements
- Getting phase loss diagnostics on compressor A and B.
- Phase loss diagnostics and Starter contactors will not pull in.
- Current Transformers (CTs) checked and resistance is ok. Less than 0.1 Ohm variation between each one and they are the same resistance as the other circuit's CTs.
- Replaced 1U4 compressor module.
Facts
- RTAA 70-125 TON (PUEBLO)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.