Low Refrigerant Temperature: The suction saturated refrigerant temperature dropped below the Low Refrigerant Temperature Cutout setpoint for 30F-sec (IOM CG-SVX17N-EN)
Causes for Low Evaporator Temperature include:
- Bad Suction Temperature Sensor (intermittent), Bad Suction Pressure Transducer
- EXV issues
- Low Water Flow-Verify design flow
- Low Refrigerant charge: Verify Subcooling (15-20 F) and EXV 40-50% open at full load, 12 F superheat; Ratio= EXV % flow command / Superheat Control Compressor Flow estimate > 1.6
- Incorrect Setting of Low refrigerant Temp Cutout (IOM). It should be set for type and percent (%) of glycol concentration
Approach Temperature is the difference between the Evaporator Leaving
Water Temperature (EWLT) and the Saturated Refrigerant Temperature
Its value represents the efficiency of the Braze plate heat exchanger.
The lower the value, the better efficiency
High approach temperatures can be the result of:
- Fouled evaporator, broken or by-passed water strainer. Flush evaporator water side with hot water
- Bad Suction Pressure Transducer, bad leaving water temperature Sensor
- Cross Bind sensors between circuits
- Water Flow too low
- High concentration of glycol
- Bad Suction Temp Sensor
- EXV malfunction
Additional details
Resource Available
- Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- IOM: CG-SVX17N-EN
Other Question/Problem/Cause Statements
- Low evaporator temp cut out
- Low Refrigerant Temperature
- High Approach
- Why this chiller has high approach?
Facts
- Chiller has high approach temperature. Approach was 35F
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.