Evaporator Water Flow Lost and Evaporator Water Flow Lost Lockout
- After the pump request was activated, water flow was established and then lost. Special action is to keep the evaporator pump request active in a diagnostic override mode.
- Evaporator Water Flow Lost Lockout is a diagnostic that occurs when Evaporator Water Flow Lost events occur 4 times within a 4 day time window.
- This diagnostic will be shown on all subsequent flow lost events unless the diagnostic does not occur within 4 days or the Main Processor (Dynaview) resets due to power loss.
- Corrective action should be taken to eliminate the cause.
Review submittal for the following details:
- IFM flow switch setpoint
- Glycol type and concentration
- Water pressure drop and flow rateValidate water flow through the chiller. Reference the submittal for design flow and pressure drop information
Verify the appropriate IFM flow switch is installed in the chiller per submittal
- Validate the orientation of the flow switch indexing dot. Refer to the Installation Operation Maintenance Manual for details
- Troubleshoot the flow switch operation, wiring to the 1A17 LLID, and the 1A17 LLID operation
DO NOT JUMPER FLOW SWITCH - Ensure the water piping has been purged to eliminate air which will cause inconsistent flow switch operation
Notes
For reference only...see appropriate wiring schematic
Additional details
Other Question/Problem/Cause Statements
- Evaporator Water Flow Lost
- Evaporator Water Flow Lost Lockout
Facts
- Air-Cooled Chiller CGAM
- Air-Cooled Chiller ACSA
- Air-Cooled Chiller ACXA
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.