RTAA chiller displays A01, there is a call for cooling, but chiller does not run.
- Validate there is a call for cooling
- Chilled water setpoint
- Differential to Start
- Validate Circuit Lockout is DISABLED
- Validate External Circuit Lockout is DISABLED
- These will cause the operating mode (menu A) to display A01 (Auto-Local)
Additional details
Other Question/Problem/Cause Statements
- RTAA chiller is in A01, there is a call for cooling but chiller does not run.
- Chiller does not start?
- Chiller will not run?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.