The low noise fans reduce chiller sound levels by roughly 1-2 dba in the lower octave bands. Even though 3 dBa is a doubling of power, the threshold for the human ear to tell the difference in sound levels is 3 dBA.
Sound attenuation on the compressors is the real deal as this attenuates the "tonal" frequencies of screw compressors. Humans pick up on tonal frequencies much easier than overall sound. Thus, compressor attenuation is truly a better "bang for the buck".
In addition, when the RTAC was designed, the standard fan was 3-4 dBa quieter than the old RTAA fan. That means the standard RTAC fan is 3-4 dba quieter than our fan on the 70 - 125 RTAA. So, in certain terms, the standard RTAC fan is a "low noise fan", just not the lowest one we have.
The RTAC option for low noise fans include blades that are 30% glass filled/coupled black UV stabilized polypropylene.
Refer to RLC-PRB009-EN for specific sound ratings.
RTAC — Sweepy Jr. Low Noise Fans
Additional details
Resource Available
- Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- Other: RLC-PRB009-EN
Other Question/Problem/Cause Statements
- Low Noise Fans
- Low Noise Fan Blade Material
- Sound Attenuation
- What are the sound ratings for the quiet fan option?
- I need information on the low noise fans.
- Comprehensive Sound Solution
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.