RTAA 70-125 or RTAC 140-500
- Internal pressure relief valve in GP or GP2 compressors are rated for 450 psi (differential) and a capacity of 17 lbmair/min.
- Note that this relief valve is from high side to low side of the compressor, not high side to external ambient.
- The valve "recirculates" the refrigerant inside the compressor if conditions ever cause it to lift.
- There is one valve per compressor.
Additional details
Other Question/Problem/Cause Statements
- GP and GP2 Compressor Internal Relief Valve
- Compressor internal pressure relief
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.