The Current Limit function allows the user to limit the maximum capacity of the Chiller unit. The user is allowed to input a current limit setpoint for the chiller. The compressor slide valve will be modulated in order to prevent the chiller from exceeding the current limit setpoint.
This function may be controlled by a Trane Integrated Comfort System (ICS) or through a generic BAS (GBAS) interface. The option provides a 2-10vdc or 4-20mA signal output to the BAS. A typical application might be to limit the Chiller capacity during times of peak load based on a request from the local power company.
Additional details
Other Question/Problem/Cause Statements
- How do you limit the capacity of an RTAA chiller?
Facts
- RTAA 70-125 Ton (Pueblo)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.